Part Number: PCM1808
I cannot find a definitive answer in the datasheet, but is it correct to follow the example application for a 0V centered audio signal? Can a 0V centered audio signal be input directly into the L and R input pins? Or is DC biasing of the signal necessary? If DC biasing is necessary, can the Vref pin be used for this?