Hello,
I'm set up to receive I2S audio data from a TLV320AIC3120. Now I'm trying to closed loop control the codec to try and match the input data rate of the I2S to the output data rate of my USB stack. How can I adjust the codec to bring these data rates into sync. I'm concerned that the Data rate of the USB will vary with different computers. I played around with making small adjustments to the PLL J.D coefficient on the fly which kind of worked, but it looks like doing this is not recommended without shutting down the PLL (which I hadn't done with my small on the fly changes). What are my options for bringing these data rates into sync?
Thank you,