Part Number: TLV320AIC3212
Other Parts Discussed in Thread: TLV320AIC3107, TLV320AIC3106
Hi,
We intend to use TLV320AIC3212 in an IP Phone design (based on Sitara AM5728) with the following analog interface:
- a headset to be connected to the headset block (IN1L, HPL, HPR, MICBIAS_EXT, etc).
- a handset mic connected on IN2.
- a hands-free mic connected on IN3.
- a hands-free mono speaker (8ohm, 0.3W) connected to SPKLP/M)
Please confirm if these connections are OK.
In addition we have a handset speaker rated at 0.015W and 150ohm impedance. Could you please suggest on which analog output interface of TLV320AIC3212 this can be connected?
A post related to this design is here:
Regards,
Thariq C P