Using the TPA3255 configured for PBTL with heatsink and 52V input bus. Circuit designed for high power, low duty cycle application closely following the data sheet and EVM recommendations. During development saw a few TPA3255 failures when device was pushed to extremes of power or temperature (not an issue), but production audio circuit occasionally showing failures at very low power levels which is puzzling. The failure shows up as a low resistance on the RESET input, usually under 50 ohms but always greater than 6 ohms. When I ohm out other points on the device, I can't find any other pins shorted. The RESET line comes from a processor with a NC7WZ16 (UDFN6) buffer in between. I have a 47K pulldown on the RESET line. When the circuit is instrumented, I see no obvious transients on the RESET line (~3.3V) or power buses. As a side note, we have had a high number of buffer failures (used on other GPIO between uP and audio circuit) that we are attributing to insufficient solder/manufacturing defect. The load is two 4 ohm speakers in parallel. Following recommended power on sequence.
Is the REST input failure a symptom of another failure on this IC or can the RESET input be easily damaged? Can you give me a set of pins to ohm out that may give me a clue to the root cause?