Hi Team,
When working with the DIT4096 configured in I2S slave mode and driven from a Bluetooth module with I2S audio outputs, do the I2S input signals need to be synchronous to its local master lock input? The DIT4096 local master clock input is 24.576 MHz. In this application. the Bluetooth module is configured as I2S master and provides BCK, LRK and SDATA as expected but is not running from the same 24.576MHz master clock.
Thanks,
Garret