Other Parts Discussed in Thread: TAS3251
Hi,
today I installed a brand new TAS53251EVM and PPC3 as described in the manual. System works fine in Stereo 2.0 Standard Processing (2.0 96K) mode, I can change
filters etc. However when I switch to any other Stereo modes the EVM config is started, music stops, but the process hangs in the 'Writing coefficient to device' phase, see below.
From there I can only kill PPC3 via Windows.
Weird thing is that the same happens if I disconnect USB cable. 2.0 96k mode goes through without any error msg, other modes hangs at the same point.
I run Win10 Pro 1903 last refresh. System sees a TI USB Audio UAC1.0 driver, v4.59.0 installed by PPC3. I run the music via TOSLINK. Board was purchased from Mouser
last week, LOT: 3409597WBG
How can I get this board working in the other modes ?
Thanks, Endre