This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS2563: SDOUT1” or “SDOUT for AEC

Part Number: TAS2563


Hello 

           Are “SDOUT1” & “SDOUT2” designed to stereo structure to connect to AEC chip?

Customer project have 2 speakers, (1) both of “SDOUT1” & “SDOUT2” are connected to AEC?  or  (2) either “SDOUT1” or “SDOUT2” is connected to AEC. 

Thank you. 

BR

Patrick

  • Hi Patrick,

    Either SDOUT should be connected to the host processor to receive echo reference data.
    Usually in stereo applications the gain is linked to keep the stereo image, thus the feedback from one device will be good for both speakers.

    Best regards,
    -Ivan Salazar
    Applications Engineer - Low Power Audio & Actuators