Part Number: DIT4192
Other Parts Discussed in Thread: SRC4392
hello,
I can't find the transformer suggested by the DIT4192 datasheet for the transmitter coaxial output, can DA101C be used for this purpose?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
We reviewed the datasheet for that product and it looks like it should work. It's meant for this specific purpose and meets some of the AEC standards. The jitter performance isn't specified like it is for the Scientific Conversion products, but that's what the AEC standards dictate so it should work. We use SC939-06 on the DIX4192EVM which is still in production.
thank you,
should I use the circuit shown in DIT4192 datasheet Figure 12 or Figure 13?
I need unbalanced 75Ω Coaxial Cable Transmission, as recommended by Figure 13, but it uses a 2:1 transformer, while DA101C is 1:1
as alternative, I could use the schematic suggested in SRC4392 datasheet Figure 89, but where should TX- be connected then?
Hi Dmitri,
Good catch - we'd missed the difference in transformer windings between the two units. One option would be to find a 2:1 transformer in the same family from Murata. Otherwise you can apply a resistor divider circuit similar to what you found in the SRC datasheet but make it differential instead of single-ended. A circuit like the one shown below would work