This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM3168A performance issue

Other Parts Discussed in Thread: PCM3168A, DIR9001, THS4521, THS4524

My customer has designed in the PCM3168A Audio Codec and is experiencing poor in circuit performance.

 I am on my second PCB spin, and I am getting very poor performance.  For this new board, we have only populated the clock, one CODEC, and input buffer, and an output buffer. Input has a low pass filter at around 15K, the output has a 7K low pass.  We are shooting for a passband of 150 Hz to 7KHz.

We are using a 32K effective sample rate, the 8MHz Codec sample clock has 2.5ps rms of jitter. I would like to see 90db or better SNR.

I have successfully interfaced a DIR9001 to the CPU and to the Audio Precision 2700 system. When I use the audio precision to inject an analog signal to the front end of the codec (the buffer amp is a THS4521 quad differential amp), the resulting SNR+noise curve results in only around 65 db signal to noise ratio. I was expecting at least 90 - 95 db from this arrangement. See the bitmap labeled "-002 codec A .bmp".

When we allow the audio precision to inject a digital test signal into the CODEC via the DSP, the output measurement of the codec, when buffered by an AD8397 is only around 60 db as well. The plot labeled "-002 codec A output amplifier.bmp" shows the output plot from the Audio Precision 2700. Again, I was expecting SNR in excess of 90 - 95 db.

Can you think of anything off the top of your head that can compromise the CODEC performance? I don't think the problem is with the buffer amps. I would not expect the input and output performance to be so similar if it was a buffer amp.  If I had not measured the jitter, I would have expected a noisy clock was the culpret, but I think 2.5 ps of jitter is quiet enough to deliver a 7K signal bandwith at over 100 db SNR.

Can you also forward this email to one of your audio experts, and have them send me a list of information they would like to see in order to get to the bottom of this.

(let me know if I need to get the schematics from the customer to forward on for you to review)

Here are the AP screen shots:

  • Todd,

    On the input filters, capacitors such as C209 (0.047uF) are hooked up to both outputs of the THS4524 devices.  When connected this way, the capacitor's center is rotating around the common - mode, and this results in the capacitor's value effectively being double.  This would mean the cutoff frequency is much higher than 15kHz, which would create problems at the input.  I would recommend reducing the capacitors to a value of 22nF for example, to ensure the cutoff frequency of the low pass filter is correct.

    Please let me know if there are additional questions/concerns.

     

    Thanks and best regards,