Part Number: TLV320AIC3111
Hello,
I'm facing problems with setting the clock frequencies on my device. I need a sampling frequency of 44.1kHz
As per my understanding, the MODEVM interface is giving a 11.2896 MHz as MCLK, PLL_CLK of around 90MHz and the internal clock dividers step the sampling frequency to 44.1 kHz.
For my application, I'm supplying a 4.096MHz signal to the MCLK from a microcontroller
The configurations I'm supplying is as follows -
R = 1, J = 22, D = 06, P = 1
By my calculations, this will give PLL_CLK of 90.3618 MHz, which is similar to the PLL_CLK as the EVM example. Do I need to change the other values such as MADC, NADC, AOSR etc? As the PLL_CLKIN is same, it shouldn't make any difference for the rest of the clock dividers right? I tried this approach but I've had no luck in obtaining filtered output. What am I missing out on?
I can PM the ProcessFlow and the code I've written if required.
Regards,
Souvik