Hello sir,
A continuous pause phenomenon is found by using TPA3221 BTL 2* 75w@4r when setting up to the maximum volume and playing large dynamic music with only one channel connecting to a speaker, and the other channel is empty ( if two channels are connected to speakers, there will not be a pause.)
TPA3221 is supplied by 27.5V, input about RMS≈ 0.5V, PK≈ 2.2V, observing that PWM duty cycle with oscilloscope sometimes close to 100%. In this case, the problem can be solved if TPA3221 i's supplied voltage is boosted to 32.5V and the maximum PWM duty cycle will be reduced to about 90%.
May I ask whether other D-class amplifiers have the same output pause phenomenon when input is overloading? Why the phenomenon is caused? Is it because of TPA3221 has different internal protection mechanism to be triggered? besides the method of using boost to promote VCC, are there some other methods?
Many thanks for your reply!