This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS2505: Handling unused pins on TAS2505

Part Number: TAS2505


About the TAS2505 data sheet (JAJSDJ0B –FEBRUARY 2013–REVISED NOVEMBER 2016) The signal name of Pin 5 in Pin Configuration and Functions in section 5 is HPOUT. On the other hand, it is NC in the table. Can I use No Connect (Leave unconnected) when the pins are unused? The analog input pins (AINL and AINR) are not used. If so, what should I do with the pins? best regards