I am having difficulty in using the DI_GET_DEVICE_INFO instruction. I first issue the CMD_REQ command with 1E instruction (i.e. 0xDE in the CMD_REQ format) then wait for MISO high then put 900C and twelve zero bytes, all with CS low. The response for the CMD_REQ and the 900C first part of READ() is correct - the status word but then I get also the status word repeated 6 times in the data part which is not what it should be. What may I be doing wrong ? Attached the first part of what I generate