Hey guys!
I need to make an MP3 (or AAC) encoder so it can be connected to Raspberry Pi over SPI interface. Ideally, I will also need an ADC.
The idea is to convert an audio into MP3/AAC and hand it over to Raspberry Pi (SPI), so it would create an .mp3 file.
Are there such an IC's and/or reference desings?
I need to point out that it must be a minimum possible power consuming solution.
Thank you.