This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM1754: Is there any test data about VCC max voltage and time for a spike?

Part Number: PCM1754

Hi, team,

In PCM1754 datasheet, VCC abs. max voltage is 6.5V. In my customer design, the VCC power rail is 5V, but in system battery drop test, the VCC pin voltage will go high as a spike, the peak value is ~7.6V, the duration of >6.5V time is ~14us. The spike is caused by system level reason and cannot be eliminated now.

Do you have such test or data on the VCC pin voltage spike about the peak voltage and time? Customer needs this to evaluate the risk to device.

Thanks.

Johnny