can i use this module(cc85xxDK/ purepath wireless audio EB) for video transmission?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Siva,
I don't believe so. The difficulty in setting up the CC8520 for non-audio data is the processing that the CC8520 does in poor SNR conditions. For example, if it misses a sample and can't recover it in time through retransmits, it eventually interpolates the sample (page 36 of http://focus.ti.com/lit/ug/swru250b/swru250b.pdf). There are also algorithms to mute the channels in a "soft" manner if packets aren't being received. This signal processing, which maintains excellent audio quality, is not appropriate for video data, and the result would probably not be satisfactory.
-GrantC