This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3111D1: high temperature

Part Number: TPA3111D1

Dear all:

        I used TPA3111D1 to do the temperature rise experiment, electrified and turned on the horn. After 20 minutes, I found that the inductance temperature of TPA3111D1, L2 and L3 was very high, about more than 100℃.Although the chip is not damaged, the temperature of this part of the chip is too high, resulting in high ambient temperature

       Attached are the schematic diagram and PCB, please help to provide improvement Suggestions?

  Thank you!

LDS-SKF-YY-01B-V2.0-Y5.zip

  • Attached are the schematic diagram and PCB, please help to provide improvement Suggestions