Part Number: TAS3251
Other Parts Discussed in Thread: , TAS5780M
Dear Support team,
I have a question about the SRC function of TAS3251.
I loaded Process Flow 1 (96 kHz, 2.0 Standard Processing) with PPC3 and checked the equalizer coefficients.
Case 1 is USB In : 48 kHz.
w 94 00 00
w 94 7f 8c
w 94 00 16
w 94 1c 00 7b fb f5 00 7b fb f5 00 7b fb f5 70 40 c3 c5 9d 8e 88 a1
w 94 00 00
w 94 7f 8c
w 94 00 18
w 94 08 08 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
Case 2 is USB In : 96 kHz.
w 94 00 00
w 94 7f 8c
w 94 00 16
w 94 1c 00 20 ed 0b 00 20 ed 0b 00 20 ed 0b 77 e2 94 c5 8f b7 22 4a
w 94 00 00
w 94 7f 8c
w 94 00 18
w 94 08 08 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
In this way, the coefficients of the Biquad filter are different.
If Process Flow 1 (96 kHz, 2.0 Standard Processing) is used, will the 48 kHz sampling rate be converted to 96 kHz ?
Or does TAS3251 process flow 1 have no SRC function?
If there is no SRC function, is it necessary to change the filter coefficient according to the input sampling rate?
Best Regards,
Hiroaki Masumoto