Hello
My customer chosen TAS6424L-Q1, but have a question below.
Please advise.
Question:
Can I have ILIMIT reporting at FAULT pin? or cannot?
Which is correct description either " 9.3.8.1" or "9.6.18"?
~~~~~~~~~
9.3.8.1 Overcurrent Limit (ILIMIT)
ILIMIT is not reported as a fault condition to either registers or the FAULT pin. Each
channel is independently monitored and limited.
9.6.18 Pin Control Register (address = 0x14) [default = 0x00]
Table 27. Pin Control Field Descriptions
Bit2 MASK ILIMIT R/W
Reset 0
0: Report Ilimit on the FAULT pin
1: Do not report Ilimit on the FAULT pin
Best Regards