Other Parts Discussed in Thread: LM49251, LM49250, TLV320AIC3107, TLV320AIC3007, TLV320AIC32
Actually this question concerns three parts
LM4947, LM49250 and LM49251.
I have 1 mono electret condenser microphone input and 2 stereo line inputs, I want to mix combinations of these which I think is possible with the above chips.
My concern is can these chips handle the number of inputs
For LM4947 I see that the input selection has a particular mode
Table 4. Input/Output Control
| L2R2 | L1R1 | SE/DIFF | |
| Select LIN1 and RIN1 Stereo Pair | 0 | 1 | 0 |
| Select LIN2 and RIN2 Stereo Pair | 1 | 0 | 0 |
| Select LIN1+LIN2 and RIN1+RIN2 Stereo Pair | 1 | 1 | 0 |
| Sets Stereo Inputs to Differential | x | x | 1 |
As seen I don't quite understand what LN1+LN2 and RIN1+RIN2 mode does?
Can I connect 2 stereo single ended line inputs Line1_L / Line1_R and Line2_L / Line2_R to the pins LIN1 / RIN1 and LIN2 / RIN2 and get the requirements done?
Will the other chips LM49250 and LM49251, be better suited for this?
I also see that these chips don't have an inbuilt microphone preamp, any suggestions for a pre-amp chip with minimal external components would be welcome!