This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM4755: LM4755-Unused pin suggestions

Part Number: LM4755

Hello Sir,

I have prepared Prototype for the LM4755 as attached below circuit.

Input conditions:

VDD=22VDC

INPUT SIGNAL:200mV (1KHZ).

Output yet not connected.

Here, problem is that

IC LM4755 is getting heat up when we powered up with 24V

Could you please let me know about the pins connections in above circuit.

INA Pin connect to?

OUTA Pin Connect to?

i have checked with following combinations

  1. INA=GND,OUTA=OPEN ,Result: IC Heat up
  2. INA=GND Via 0.1uF,OUTA=OPEN -IC Heat up
  3. INA=OUTA=GND=IC Heat up.
  4. INA=OUTA=BIAS Pin-No Heat up, but Bias pin voltage reduce to 1.5V (Instead of Half VDD) and output clipping.

I did not get the Any statement in the Datasheet?

Regards,

Deepak