This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3111D1: FAULT AND SD pin to 0V when i connect Plimit to gVdd

Part Number: TPA3111D1

Hi,

I can't make the TPA3111D1 work correctly. When i connect gVdd to plimit the TPA3111D1 shutdown (SD and FAULT pin to 0V) but when i let the plimit floating the TPA3111D1 starts. And when i start the TPA3111D1 with plimit floating and then i connect plimit to gVdd, the TPA3111D1 works correctly with no output limitation. I also try to put 2V at plimit but the amplifier doesn't start. Thanks in advance for your help.

Pierre.