Other Parts Discussed in Thread: TPA3251
Hi,
I got two questions about TAS3251.
- TAS3251 has a 'RESET_AMP' pin but it seems only ramp down the output stage and reset the error message. Is there an 'traditional' hardware reset pin in TAS3251? What I mean 'traditional' is all the register value will be reset as well. In the datasheet page 21 - functional block diagram, we can see a reset pin (looks more like a traditional reset pin) in the bottom left besides the reset_amp# pin in the bottom right.
- Is there a more detailed datasheet which includes the register page to 255? The current datasheet only cover register page 0 and 1. However, functions such as fine volume control is located in page 21, and there is no DSP function mentioned in the registers in page 0 & 1 as well.
Thank you!
Best regards,
Joe