Part Number: TLV320AIC3104
Other Parts Discussed in Thread: TLV320AIC1110
Team,
I saw this E2E post that suggest that the MCLK is not alaways needed.
Could you please confirm if the below scheme is ok to use?
Also what are the features/functionality that might be altered if MCLK is not used?
Can it sample in PCM 8bits (uLAW ou ALAW) ?
-CLK for TDM:
Here is the setup:
-Two AIC3104 for a total of 4 IN + 4 OUT channels:
16 bits to TDM bus (16-, 20-, 24-, or 32-Bit Data)
-Clock: 8Mhz, FS: 16kHz
Fig 17 of the SLAS510F Datasheet suggest that BCLK can be used for ADC/DAC clocking (see picture below) however I saw that in the SLAA469A app note (Fig 2, Fig 4) that the ADC itself it clock by MCLK.
-Can you confirm that this scheme is possible without MCLK?
-what are the features/functionality that might be altered if MCLK is not used?
Thanks in advance!
A.