This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5751M: Some settings cannot be written

Part Number: TAS5751M


Some settings cannot be written
I changed the following address
but,Some do not change
(Writ settings)
0x51 00 80 00 00 00 80 00 00 07 80 00 00
0x52 00 80 00 00 00 80 00 00 07 80 00 00
0x27 00 82 01 6c 07 09 a7 2e 00 7b 57 66 00 f6 58 d2 07 82 a7 2e
0x31 00 82 01 6c 07 09 a7 2e 00 7b 57 66 00 f6 58 d2 07 82 a7 2e
(Read settings)
0x51 00 80 00 00 00 80 00 00 03 80 00 00
0x52 00 80 00 00 00 80 00 00 03 80 00 00
0x27 00 82 01 6c 03 09 a7 2e 00 7b 57 66 00 f6 58 d2 03 82 a7 2e
0x31 00 82 01 6c 03 09 a7 2e 00 7b 57 66 00 f6 58 d2 03 82 a7 2e
What can't be changed?
please tell me
Best regards
  • hello Sir,

        Can you let us know do you use TI PPC3 to write register or by other end user I2C written tools?

    Regards

    Linda

  • Hello customer,

    Please debug by:

    1. To confirm the I2C address
    2. Use your I2C tools to confirm whether NACK occurs during I2C communication;
      1. If your Tools cannot find NACK, then please scopes I2C waveforms to me for analysis.

    3. To share how you write this commands by capture some pictures to us.

    Regards,

    Alix Wan.

  • I created a set value using PPC3
    and,I use a different writing method than PPC3

    1. I Create Settingfile(TAS.csv) with setting values written
    2. Transferring settings to devices that already have TAS5751(via USB_Memory)
    After reboot
    Some differences when reading set values from the device

    I looked for a setting that would be the value read using PPC3 but could not find it.
    What is the difference between the settings I wrote and the settings I read?
    Please tell me

    Best Regards

  • Hello customer,

    Is there any update? Please come to us after your have more update.

    Regards & Thanks!

    Alix Wan.