Part Number: PCM5122
Other Parts Discussed in Thread: PCM5102
Hello,
I'm using a PCM5122 (and previously a PCM5102) in my design and I've had a couple of prototypes end up with the 3.3v rail shorted to ground. A little investigation has yielded that the CPVDD pin is bringing the rail near ground. Similarly, the VNEG pin has only 20k ohm resistance to ground. No other pins appear to be shorted. The outputs of the DAC connect directly to an onboard amp, as well as being tee'd off into a vehicle amplifier.
My question is this: What could cause this kind of damage to the DAC? I have not done anything outside the box with the implementation, other than change the output filter to supply a higher output load.
Here is my schematic:
Here is the layout for this part, including where one channel is input into a small audio amp.
Thanks!
-Ted