Other Parts Discussed in Thread: TPA3139D2
Hi team,
My client now wants to make a voice module which is used in the home appliance to recognize and output voice
For this project, he has the audio PA selection requirements. Please see if there are any recommended audio PA in this application.
-
VDD: 12V, THD+N < 0.1%, SNR > 85dB, Speaker: 10W@4Ω
-
Working temperature: - 40 ° C ~ 85 ° C
Best Regards
Wesley Huang
wesley-huang@ti.com