Other Parts Discussed in Thread: TLV62568A
Hi team,
My client now wants to make a voice module which is used in the home appliance to recognize and output voice, so he need the two DCDC to supply the MCU and OP.
For this project, he has the two DCDC selection requirements. Please see if there are any recommended two DCDC in this application.
-
Vin:12V, Vout:5V,Iout:500mA, Vo_ripple < 30mV. Working temperature: - 40 ° C ~ 85 ° C
-
Vin:5V, Vout:1.8V,Iout:500mA, Vo_ripple < 30mV. Working temperature: - 40 ° C ~ 85 ° C
Best Regards
Wesley Huang
wesley-huang@ti.com