Part Number: TLV320DAC3203
Hello:
I want to know the value of amplifier gain, it is covered by black block ,thank you so much !
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TLV320DAC3203
Hello:
I want to know the value of amplifier gain, it is covered by black block ,thank you so much !
Hi,
The amplifier gain is actually configurable. You can set a gain value in the range of 0dB to -72.3dB. Also, you can set the value to MUTE. The register that configure the gain for INL is located in page 0 / register 22 (0x16). The register associated to the gain for INR is located in page 0 / register 23 (0x17).
http://www.ti.com/lit/ug/slau434a/slau434a.pdf#page=109
Please let me know if you have additional questions or comments on this. We will be glad to help you.
Best regards,
Luis Fernando Rodríguez S.
Hi sir. :
Thank you for your reply!
One thing want to consult you: why is the amplifier gain less than 1 (0dB to -72.3dB)?
I think if we use analog microphone sensor it will create very small signal, designer need an additional amplifier to make signal big enough. So, why is the amplifier`s gain less than 1? maybe we need the amplifier gain greater than 1, maybe +20db or +40db. and designer will save the additional amplifier and cost down.
Thank you so much!
Hi,
Usually, these analog inputs are not used for microphone purposes. They are designed to connect a line signal, which uses to be higher than a microphone signal. That's why an amplifier with lower gain is used in this design. If a higher gain is required, the headphone amplifiers can be configured with a gain from -6dB to 29dB as shown in the block diagram.
For more details, please consult page 1 / registers 16-17.
Best regards,
Luis Fernando Rodríguez S.