Other Parts Discussed in Thread: TPA3128D2, TAS5805M
Hi
If the speaker transducer has been chosen as 2 ohms @ 25 watt or @ 20 watt . Is the TPA3132D2 good choose to drive this transducer ?
( I assume we can use the 19V as VPP input )
Since checking from datasheet
1. it mentions 2 × 25 W into a 8-Ω BTL Load at 19 V ;
2. Section 6.3 ; mentions about the minimum load impedance requirement as BTL structure w/ 3.2 ohms above and PBTL w/ 1.6 ohms above .
Would you please help answer what is the majority factor to impact the load impedance selection ( 2 ohms )? And how to calculate ? Thanks
ARSIR