This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5825M: Question of Processing Rate of DSP_CTRL Register of TAS5825

Part Number: TAS5825M

Hi Sirs,

Can we write 0x46 = 0x01 for every TAS5825 projects to support 32kHz sample rate? Any side effect?



Thank you and Best regards,

Wayne Chen
12/19/2019 

  • Hello Wayne,

    In our PPC3 GUI, you can choose "As input" to adjust for different sampling rate. For SRC module, "As input" can support 32, 48/44.1, 88.2/96 and 192KHz.

    But it is suggested to choose the process flow and set that in process flow.

    Regards,

    Alix Wan.