Other Parts Discussed in Thread: TPA3255
Dear again I'm not sure that the 10uH give more power than the 7uH, on my measurement it seems almost equal.
Could you just explain me this double pole just to be sure to understand?
When you decrease a capacitance in a filter, the cutoff frequency increase, right?
Then why on the PFFB application note the capacitance C_FBout is higher when the switching frequency is @ 600kHz than 450kHz.
I try to understand how this system work with this T filter.
Another thing I try is the different mode MST,AM1,AM2 without PFFB first, every circuit seems to work properly in his own base frequency.
When i try to use the AM2 i get some issue on my results.
TPA3251 with 7uH 680nF or 10uH 1uF --> Master mode perfect (600kHz)
TPA3255 with 7uH 680nF or 10uH 1uF --> Master mode perfect (450kHz)
TPA3251 and TPA3255 with 7uH 680nF or 10uH 1uF --> AM2 some THD+N issue vs output power, spikes
Is it normal? The LC filter with this value work only for the master frequency? is it needed to adapt the output filter with different mode?