Part Number: TLV320AIC3110
Hi,
I'm new to using the TLV320AIC3110 and have been trying to get basic headphone operation working using the Example Register Setup to Play Digital Data Through DAC and Headphone/Speaker Outputs documented in section 7.3.10.14 ( p64-65 ) of the datasheet. As I as going through the example I noticed an odd set of instructions. I'm wondering what the purpose of the 4th and 5th last instructions are?
They read:
w 30 00 08
w 30 01 04
From my understanding this would mean, change to page 8 then write 0x04 to register 1. However register 1 in page 8 is reserved with a note "Reserved. Do not write to this register." Am I missing something or is this instruction incorrect? Is there possibly a slightly different set of instructions here that are required?
Kind Regards,
Jon