Other Parts Discussed in Thread: TAS2505-Q1
Can you suggest an external circuitry for open load detection in TAS2770?
Regards,
Anjanaa
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can you suggest an external circuitry for open load detection in TAS2770?
Regards,
Anjanaa
Hi Anjanaa,
You can use the circuits from this AppNote as reference for open load detection.
Best regards,
-Ivan Salazar
Applications Engineer - Low Power Audio & Actuators
Hi Ivan,
Thanks for the appnote.
From the Appnote suggested regarding open circuit detection, I am using Diagnostic Circuit #2 with BJT and MOSFET suggested for TAS2505-Q1 amplifier.
The suggested amplifier IC has a GPIO pin as given in appnote, but we are using TAS2770 amplifier, which does not contain the GPIO Pin, so we are using micro-controller GPIO Pin is used for output and Input. Attached the circuit for reference.
Here we try the two types of configuration. We are expecting to achieve configuration, but audio was not able to detect.
Configuration 1:
This behaviour happens as expected.
Configuration 2:
1. Mute the audio amplifier
2. Then verify the open circuit
3. Unmute the amplifier IC
4. Make TAS2770 to play – But audio was not detected
The actual working scenario should be as configuration-2 whereas we are facing issue in it.
Kindly let us know how to address/debug the issue in 2nd configuration.
Hi Anjanaa,
Can you explain further the differences on config 1 vs config 2? Is it only config 2 does not have step 3 from config 1?
Can you read registers 0x24, 0x25 and 0x26 to check if there is any flag being triggered?
Best regards,
-Ivan Salazar
Applications Engineer - Low Power Audio & Actuators
Hi Ivan,
Can you explain further the differences on config 1 vs config 2? Is it only config 2 does not have step 3 from config 1?
Configuration 02 |
Configuration 01 |
1) Mute the device. 2) Enable the GPIO 3) Delay for 100ms 4) Read the input for speaker present 5) Disable the GPIO 6) Play the audio 7) Check short 8) Disable the device
|
1) play the audio 2) check short 3) disable the device 4) Mute the device. 5) enable the GPIO 6) Delay for 100ms 7) Read the input for speaker present 8) Disable the GPIO
|
State of Registers 0x24, 0x25 and 0x26:
While increasing the delay from 350ms, the audio cannot play.
Above 350ms delay, checked the register values,
Register values are:-
PWR_CTL - 0x00
MISC_IRQ - 0x80
INT_LIVE0 - 0x04
INT_LIVE1 - 0x00
INT_LTCH0 - 0x04
INT_LTCH1 - 0x00
INT_LTCH2 - 0xC3
Thanks,
Anjanaa
Anjanaa,
From register INT_LTCH0 = 0x04, it seems there is TDM clock error. Can you scope your SBCLK and FSYNC to check if these signals are missing at one of the steps you listed?
If these signals are missing at some point, you could try to disable the device (using register 0x02) before the signals are missing, and re-enabling the device after these signals are back.
Not sure if it's just a missing step, but in step 1 it is "Mute device" but I don't see any "Unmute device" step prior to "6) Play the audio"
Best regards,
-Ivan Salazar
Applications Engineer - Low Power Audio & Actuators