This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3221: output power issue

Part Number: TPA3221

Hi Sir

could you help check above questons and give some way to solve issue,tks!

when we use 1KHZ signal as input, the output power can reach 85W under the conditions of BTL module, however, if we use 4KHZ or more than 4KHZ signal , the TPA3221

only output 25W, if more than 25W power it will distortion,what's more, we also use AP to test, it is the same issue, LC circuit:L=15uH,C=1uf;we also use L=10uH,it is Same invalid

only when the input signal is 1KHZ, it will normal,the SCH as follow, could you help check it and give the suggestions for this qustions,thanks!