Part Number: TAS5717
Hi Team,
When MCLK = 512fs at Fs: 48kHz, it becomes 24.576MHz,
In this case, there is no margin, I would like to confirm.
If you have a margin, can you tell me the upper limit?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TAS5717
Hi Team,
Hello Shidara,
You can configure MCLK=512Fs=24.576MHz without concern. The maximum/min value for MCLK listed in the datasheet is mainly for the limit of configuration.
For example, when MCLK=512Fs=24.576MHz, if variations occur in Fs, eg Fs=48.2MHz, then MCLK= 24.68MHz. This kind of variation is ok. But if MCLK = 513 or more * Fs, it is not allowed.
Regards,
Alix Wan.
Hi Matthew-san
Thanks for your advice.
Because the maximum/min value for MCLK listed in the datasheet is mainly for the limit of configuration only,
is it possible to indicate the tolerance of variation including jitter?
ex) Within plus or minus 1%.
Thanks
Best regards,
Shidara
Hello Shidara,
Most Crystals have a frequency tolerance less than 30ppm and stability less than 50ppm. This should be fine for our device.
Best Regards,
Luis
Hi Luis,
Thanks for your comment.
Since the audio CLK is generated by decoding the audio data superimposed on the video signal,
it contains a large amount of jitter when compared to a crystal oscillator or the like.
If you could indicate the permissible variation, it will be helpful for the customer.
Thanks in advance.
Best regards,
Shidara
Hello Shidara,
When you say it contains a large amount of jitter, can you specify an amount?
All the best,
Carolina
Hi Carolina,
Thanks for your support.
Jitter will be +0.71%(max).
(24.75MHz / 24.576MHz)
How is it?
Thanks
Best regards,
Shidara
Hello Shidara-san,
If your MCLK variation is between 24.576MHz - 24.75MHz than that should be okay even though it is above the max parameter of the datasheet.
Would not recommend anything higher than 24.75MHz.
All the best,
Carolina
Hi Carolina-san
Thank you very much for checking.
I understood. Let me inform this to my customer.
Thanks
Best regards,
Shidara