This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM49450: constant component at the HP outputs

Part Number: LM49450

Hi.

I have constant positive voltage at the outputs HPL and HPR. ChargePump frequency 323375 Hz (measured on C1N), CPVdd and HPVdd - 2.5V, IOVdd, DVdd, Vdd, LSVdd - 3.3V. On HPVss i have +0.4V. What voltages should be at such power voltages at BYPASS, REF and HPVss pins?