Hi.
I have a problem with interfacing TLV320AIC3100EVM-U Evaluation module with my PC via USB cable. I have installed the slac366a software and run CodecControl.exe. When I connect the evaluation module i get an error: "'680.0' is not a valid floating point value" and an empty progress bar in the backroud. When I click OK, only the empty progress bar is shown.
If I select the EVM simulation the same error message appears.
I am running Windows XP SP3. Same problem accured on another computer. Both are TOSHIBA notebooks.
Please help.
Thank you,
Jernej