Other Parts Discussed in Thread: OPA861, TLE2426
Hello,
I'm a little bit confused about the quiescent current of the OPA861.
Im my application, I'm using the OPA861 in a single supply configuration with 6.6V DC.
I'm also using a TLE2426 as a Vbias to improve the distortion.
From the data sheet, I understood that there is a built in 250 Ohm resistor, If that is correct, I should be able to connect the OPA861 Pin 1 driectly to GND ?
But I plan to use an external 47 Ohm from Pin 1 to GND in order to encrease the quiescent current and decrease THD, is it OK ?
Last one, What about using the TLE2426 as a rail splitter as shown here ?
Jean