I am trying to run through the steps required to tune the Echo Cancellation and the instructions want the signal levels of the I2S data recorded so the dB levels can be determined.
For the life of me, I can not get probe points in PurePath 4.8 build 1 rev 10211 to work. If I add 1 probe point it won't show up in the data point window. If I add a second that one shows up and sometimes works, if I add a third one that also won't show up.
Has anyone else seen this problem and found a workaround?