This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, is it possible to simply share I2S bus between DIR9001 and PCM1794A with resistors in the path, or is it necessary to use multiplexer? In case of multiplexer, which part would be recommended, assuming auto switching is required, with priority given to DIR9001 with toslink input.
Hi Nebojsa,
You will need to have some kind of switch between the two. If both devices were sourcing a signal (which they usually do, just with zero data), then there will be conflicts. I recommend a simple digital switch, and you can try to use the DIR9001's ERROR flag as the input. This way when a valid TOSLINK input is applied, the switch will change sources. A simple device like the SN74LVC257ARGYR can be used for the switch.
Thanks,
Paul
Hi Paul,
Thanks for the answer. Do you think ERROR flag is a good indication for present audio signal, or should I use !AUDIO instead? Also, I guess I could also use SN74LVC157 instead of *257?
Thanks,
Neb.
Hi Neb,
If you expect the input to always be audio (linear PCM data), which i think is reasonable given your application, then AUDIO will work for the logic switch as well. The SN74LVC157A will work as well. Seems like a pretty cool project!
I'm following the thread over at DIYaudio as well. :)
Thanks,
Paul