This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA6130A2: TPA6130 Internal Feedback Resistance

Part Number: TPA6130A2


Hi Sirs,

We are collaborating with customer to optimize pop noise of the TPA6130 with I2C. Would you pls advise the internal resistance of input and feedback network as a following of the thread at "https://e2e.ti.com/support/archive/internal/int-audio_amplifiers/f/8/t/330999"?

Does the I2C volume control done on resistor network of input or feedback? We are considering to add external input resistance and adjust DC block capacitance to optimize the frequency response and pop noise.



2.2uF Input cap -> Pop noise but flat frequency response



0.47uF input cap -> Redued pop noise but low band impacted



Thank you and Best regards,

Wayne Chen
01/22/2020