This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC8520 sample rate ?

Other Parts Discussed in Thread: CC8520

Hello , dear

CC8520 Solution , 

Aplication apply : Wiress Mike

Qustion) Sampleing rate time reduce ?

                 example ) 768sample = 17.4ms

               So reduce time ?

               How  can reduce time? (Max time)

 

thank you

 

  • Hi Kim,

    The audio latency in an CC85xx  can be configured between 768-2048 samples. Thus, the minimum latency using 768 samples and a sampling rate of 48 kHz is 16ms and it is not possible to go any lower than this.

    Regards,

    Pelle