This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA2500: EVM set-up / issue with parallel interface

Genius 17455 points

Part Number: PGA2500
Other Parts Discussed in Thread: PGA2505

Hi all

My customer is looking at the PGA2500 / PGA2505 and has bought the EVMs. So far they haven't been able to make this work due to the parallel interface and SW that is only running on legacy operating systems. They did buy a USB-to-parallel port adapter but were not successful with this.

Can you help here ?

Can you document a configuration / set-up that works ?

Best regards

Ueli

  • Hi Ue,

    Thank you for your post. I can help you.

    Can you clarify which USB-to-Parallel port adapter they bought? The ones we've seen are for printers. So while it may fit, the connections are NOT the same so it will not work with the PGA2500 /PGA2505 EVM.

    We are looking into updating this EVM to have a more modern solution with a USB. 

    Another option could be to buy a parallel port card that can be installed into a tower of a computer.

    -Tamara

  • Hi Tamara

    Thank you for the quick reply. I will follow-up by EMail with you.

    Best regards

    Ueli