Kai, kindly answered my query regarding the use of LM4766 as an Ampifier using the link attached.
He stated "You can close S1 permamently, if you don't want to mute the LM4766 by hand." As he did not offer a value for Cs, may it take it that it is the same value as Cm?
He also did not comment specifically on my end impedance being typically 175 Ohms to 200 Ohms rather than 8 Ohms, and I still wonder whether I need to add some form of resistance etc to compensate?
CJJ