Part Number: TLV320AIC3105
Hi Team,
My customer is reviewing the startup sequence (register setting order) of TVL320AIC3105 now, because they have some issue on their TLV320AIC3105 system. But they did not understand the startup sequence (register setting order) from the TVL320AIC3105 datasheet.
Could you describe the startup sequence (register setting order) of TVL320AIC3105?
* Especially, they want to know the setting procedure of PLL. Because they are worried that if the PLL operates in the middle of setting, it will be unlocked and will not lock after setting.
<Issue>
- The following situations may occur when the power is turned on. (Frequency is about once every 30 times)
- Pulse noise is always generated in ms cycle
- Improve by restarting the power supply or re-executing the IC startup sequence.
<TLV320AIC3105 system>
- /RESET pin and Registers (through I2C communication) of the TLV320AIC3105 are controlled by ARM processor (ARM Coretex-A9 processor integrated in Xilinx Zynq
- Clock setting of the TLV320AIC3105 is,
MCLK: Input
BCLK: Output
WCLK: Output
- Audio digital line is connected with PLL block of Zynq through I2S
Thank you.
Best Regards,
Koshi Ninomiya