This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA1622: Output power, reference ds Figures 38/39 Output voltage vs Output current

Part Number: OPA1622

Hello TI!

Regarding datasheet and output power.

Root issue: Is the X-axis mA RMS, DC, or Peak?

Referencing Figure 38 and 39 of the OPA1622 ds, it appears that ±18 V rails are used to drive ~16 V dc (or 16 V peak?) in to ~120 Ω load, resulting in approximately 130 mA output current.  Do I understand correctly thus far?

On my prototype, I'm measuring 85 mA RMS, and ~120 mA peak at threshold of distortion.

Kind Regards,

David McRell