Hi Everybody , ı will appreciate your support on this, I am designing an amp using TPA3116D2 with BTL mode 2 x50 watt, With one switch i want to put the amp into PBTL mode to drive 70/100 Volt transformer handling 100 Watt.
With this switch , i am grounding İnpL and InnL . I am appliying the analog signal only to Right Amp input . And shorting the OUTPR & OUTNR together with OUTPL & OUTNL respectively with a dpdt Relay. Will shorting these pins while in BTL mode will trigger a fault in the circuit?
it s written that you need to power up the amp for PBTL operation, can i activate the PBTL operation putting the amp to SDZ low and high again? i will apreciate if you have had such an experience before to comment on this?..
Thank you