Hi, We are looking for a Codec part which should support the Bandwith = 300 Hz … 3 kHz; Max Level = + 6dBm Output. Can you please suggest the part?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, We are looking for a Codec part which should support the Bandwith = 300 Hz … 3 kHz; Max Level = + 6dBm Output. Can you please suggest the part?
Nandhini,
This isn't much to go on. What are you using the codec for? Do you have requirements for control? (ie hardware controlled, I2C,SPI?) what Audio Serial interface format is required? do you require any onboard processing? do you want a codec with USB functionality? etc...
we have a pretty broad codec portfolio with a large number of devices, so the more information you provide the easier it will be to find a match.
best regards,
-Steve Wilson
Hi Steve-Wilson,
Thank you for your response
We are Looking for a Audio Codec and amplifier which should meet the Bandwidth = 300 Hz … 3 kHz & Max Level = + 6dBm and also it should have proper isolation. Codec should have I2S Interface & I2C Interface. We don't want Codec with USB functionality.
Regards,
Nandhini
Nandhini,
Here is a link to all of the Codecs on TI.com.

As I mentioned we have a broad codec portfolio, your requirements are not very specific.
best regards,
-Steve Wilson