Part Number: TPA3126D2
Other Parts Discussed in Thread: TPA3116D2, TPA3130D2, TPA3118D2, TPA3220, TPA3128D2
I have been testing a TPA3126D2EVM eval board for an upcoming project. Relevant information: 400kHz switching frequency, gain is 26dB, PVCC is 24V, no PLIMIT set, and I'm using an AP2700 for signal generation and loading/analysis.
My goal is to be able to drive a 20W/4Ω continuous 1kHz sine on both output channels while staying at or below 100°C on the chip. This is certainly possible with the eval board's provided heat sink, ATS-TI1OP-521-C1-R1; however, it is much too large for our future design, which will be placed within a small enclosure with multiple other PCBs. Are there other heat sinks that you could recommend that have a lower vertical height (maybe closer to 0.5") that work well with HTSSOP packages?
I've had difficulty looking for heat sinks specifically for HTSSOP or TSSOP online. I've tested a few BGA pin fin heat sinks with the eval board, but they either didn't provide enough thermal relief or were comically over-sized or awkward fitting.
Or is there perhaps another TI chip that has better thermal performance for this application? Sorry for any lack of details!